Flow Sensor Locations (VAV-DD Subordinate) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The three selection options determine the specific Input names created for the flow inputs and the Setpoint/Miscellaneous modules, and the connection interfaces from the flow inputs required to calculate Hot Deck, Cold Deck, and Total Flows.

The selection options for Flow Sensor Locations are:

  • Hot and Cold Deck Flow

  • Hot Deck and Total Flow

  • Cold Deck and Total Flow