Temperature (VAV-SD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

All applications require a zone temperature sensor. This input defaults to a SAB signal to use a net stat and not consume additional IO points. The Setpoint Adjust option allows you to choose either Common Setpoint Adjust or a Warm Cool Adjust. You may also optionally select to add Temp Occ Support to include an input for temporary occupancy requests.