Optional Features (VAV-SD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Optional Features selections provide Network Inputs modules for supervisory system interfaces to override the main applications sequence of operation through connections to the appropriate Setpoint/Miscellaneous modules or State Generators.