Window Switch (VAV-SD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This option creates a hardware input WINDOW-S that indicates if a window is open or closed. The status of the window changes control of setpoints and minimum flow determination in Guideline 36 compliant applications.