System Request Generation (VAV-SD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This feature provides support for cooling temperature requests, heating temperature requests, and an option for request accumulation. You can add cooling reset, cooling plant, heating reset, and heating plant requests as network outputs that can be mapped to supervisory control.