Energy Hold Off (VAV-SD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This option allows the unit to shut down based on the energy hold off Network Input. If Energy Hold Off Switch is selected in the Misc (VAV-SD) section, then the Network Input or the Hardware Input (BI) can activate the mode. This feature is typically used to shut down the temperature and airflow control when a window or loading door is open (for example, a window switch).