Heating Flow Reset (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The heating flow setpoint increases after all types of heating selected have reached their maximum value. In certain situations, additional heating can be achieved by allowing an increase in the airflow across the heating coil.

In a Guideline 36 configured application with Box Heat selected, Heating Flow Reset is required and selected by default.