Occupancy (VAV-DD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for Occupancy are:

  • Always Occupied: This option sets the default value of Occupied for the ZN-T Setpoint Determination and Balancer Override modules to Occupied.

  • Scheduled Occupancy: This option creates the interface for the Supervisory system scheduling logic.

    • Override Support: This option creates the local override interfaces from optional Occupancy Sensors or Networked Sensor Temporary Occupancy interfaces.