Saving a Controller Application File - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. On the File menu, click Save. The Save dialog box appears.
  2. Accept the default name or type a name for the file and click Save. Invalid characters include:

    : * ? " < > | / \

    Note: The default location to save a CAF is C:\Users\<username>.