Closing a CAF - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
To close a CAF, select Close on the File menu. If you made changes, the tool opens the Save Confirmation dialog box prompting you to save. Click Yes to save the changes before closing or No to discard them.
Note: You must be in Configuration mode to close a file. You must stop Commissioning mode to remove a system from the UI.