The Control tab is part of the Classic View workspace. See Control Tab in the Classic View Workspace. See the Modes section for information on the modes of operation.
|
Screen Area |
Description |
|---|---|
|
Module Sections |
Modules used in the selected system in categorized sections. The flow of the content is from left to right where the inputs appear on the left, control/logic/state components are in the center, and outputs appear on the right. The module categories in the Control View are: |