Configuration - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Configuration mode is the default mode. When you add or select a system, it opens the system in Configuration mode. This mode allows you to design and edit a system. Configuration tasks include selecting a system, modifying parameters, creating custom logic (as necessary), and other tasks to set up a system. See the Configuring a System section for details.

The Configuration mode acts as a transitional mode when you need to switch from Simulation to Commissioning mode and vice versa. See the Changing Modes section.

Back to Modes