Outputs - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The outputs category appears in the Control tab (Figure 1). This section lists the outputs defined for the system. An output defines an interface to the actual hardware in a system. An output can represent a physical hardware point in the system or a point associated with an output. Outputs send data to hardware output points of a device.

During simulation and commissioning modes, the Output category displays a second row of text. This row provides the Output present value.

See Output Modules for information.

Back to Control Tab Module Categories