Problem |
Solution |
---|---|
When making changes to an application in
commissioning mode an Alert dialog box displays the following
information:
|
This specific behavior can be observed when making certain changes to a 6.2 application in commissioning mode without having the 6.2.2 firmware patch installed. Always apply the latest patch of firmware if you configure your applications with newer tool versions. |
Applications configured as VAV type fail download at 99% and the
controller shows a status of |
Check your CFM values for control and application configuration. VAV applications limit the MAX CFM Flow to 9,999 with a maximum 9.9 inch inlet connection. CCT does not support VAV applications where Box sizes are greater than the above stated flow and inlet size. Any attempt to configure applications for VAV Box sizes 10 inches or larger with 10,000 CFM air flow or greater will result in an application download failure to the configured controller. To accomplish a successful configuration for this VAV Box size the application will require customized or modified logic with related modules and connections. |
The Zone Temperature control does not seem to react as quickly as expected when it is in unoccupied mode. The zone temperature overshoots the unoccupied heating or cooling setpoint during unoccupied operation. See Figure 1. |
The Satisfied Timer Duration value of the Unoccupied Sequencing (VAV) is set to too high. Reduce this value to decrease the overshoot. The Satisfied Timer Duration works as follows: When unoccupied, the zone temperature is monitored to determine when the temperature exceeds the band specified by the two unoccupied temperature setpoints. When this occurs, the Unocc Status is set to the appropriate heating or cooling state. The module remains in this state until the appropriate setpoint has been satisfied for the Satisfied Timer Duration. After that period of time, the status is set to Satisfied. |
Figure 1. Changing Satisfied Timer Duration
|
|
The zone temperature cycles too frequently during unoccupied operation, and the Unocc Status changes too frequently. |
The Satisfied Timer Duration is set too low. Increase this value to reduce the cycling. The Satisfied Timer Duration works as follows: When unoccupied, the zone temperature is monitored to determine when the temperature exceeds the band specified by the two unoccupied temperature setpoints. When this occurs, the Unocc Status is set to the appropriate heating or cooling state. The module remains in this state until the appropriate setpoint has been satisfied for the Satisfied Timer Duration. After that period of time, the status is set to Satisfied. |
While making connections, one of the following error messages appears:
|
Add a Last Value block to break the unsupported loop. This process provides the information to the controller regarding where to start calculating values in this loop. Note: Within a state in a Hybrid Activity, you can create a loop without a Last Value block when connecting an output of the state back to an input of a block within that state.
|
There are no Pressure Dependent VAV Control paths to let you easily apply the VMA16 or PCV16. This path is used when no internal VP transducer for airflow control is needed. No airflow measurement. |
Set the Min Value for the VP input to a value greater than zero. This causes this input to always be unreliable, and the standard Pressure Independent application reverts to Pressure Dependent operation. |
There is no path for Constant Volume VAV airflow control with CO² sensor reset only. An example of using a Single Duct VAV application with a constant volume of airflow would be when the VAV Box is providing Ventilation Air to fan coil units. In this scenario, the VAV Box does not have a temperature control requirement. |
Set the Min Flow = Max Flow. |
There is no VAV Heat or Cool Switchover Mode path VAV heating or cooling action based on AHU supply air temperature. |
This option is available as the Warmup Mode. This mode can be implemented with a network input for supply air temperature or an supply air temperature analog input. |
The controller is not able to maintain setpoint. |
If the controller is operating while the physical system cannot respond appropriately, the controller tunes to unrealistic values. Use the Network Input Tuning Reset to set the tuning parameters to the initial values. |
The Mixed Air Damper does not open. See Figure 2. |
Due to a change in the Mixed Air Low Limit operation, the Low Limit PID starts at 0%. When Low Limit is not present, the Low Limit Process Variable and the Low Limit setpoint are the same. Because of this, the Low Limit PID does not integrate to 100%, and the output to the Mixed Air Damper is set at 0%. By changing the Low Limit Process Variable to 13 °C, 55 °F, it is now above the Low Limit Setpoint. The Low Limit PID integrates to 100%, and the damper is allowed to modulate.
Note: This fix is relevant for Release 6.0 and earlier. Release Mode 10.0 / Firmware 6.1 and later include the fix.
|
Figure 2. Adjusting the Proportional OA Damper Control V50
|
|
When simulating or commissioning a custom application in version 5.0 or later, one of the output modules shows ???? and the module details indicate an initialization error. |
Manually update custom applications and modules that include the PID block or PID pre-processor to reflect version 5.0 and later.
Note: To modify Timer block modules, delete the current Timer block, and replace it with a Timer block from the pallet.
|
More information about Adaptive Tuning is needed. |
The following guidelines should be followed when using PRAC+ Adaptive Tuning:
For more information, see PID/PRAC Commissioning Overview section. |
Romutec Hardware Inputs and IOM BI points look unreliable when you download a FW 8.0 Controller with the Disable Logic option. Although the HW value of an input follows the real status, for example, HW On, the SW value is shown with question marks, for example, Off???. This status may mean the Romutec module does not communicate with the controller. Controllers and IOM HW points are always presented with SW values without ???. |
When logic is disabled, only the execution of the sensor primitive's initial CLASSEXECUTE Method is performed. This means the Sensor Primitive cannot update its own Reliability Attribute to RELIABLE. It remains set to UNRELIABLE until logic is enabled. The question marks indicate the unreliable status during CCT commissioning with logic disabled. To fix this problem, use the Online Operations Tool to enable the logic and then disable it again while in commissioning mode. |