Users have the ability to change a controller's Computer Name and Instance Number when performing a transfer to an IP device.
Note: Do not assign an Instance Number of 1 to a controller because it is reserved for the tool.
To Update a Computer Name During a Transfer to Device
- In the Transfer Files window, click the Computer Name combo box in the New Information column.
- Enter a new computer name or click the down arrow icon for name suggestions from the CAF.
- Specify the changes required for Transfer Operations. See Step 5 in Transferring to a Device for further information.
- Click Finish. When the Transfer to Device completes, your Computer Name is updated.
Note: There may be a delay in the Computer Name updating due to system DNS caching. To work around the delayed DNS caching, run
ipconfig/flushdnsin a command line to immediately flush the DNS and update the Computer Name.
To Update an Instance Number During a Transfer to Device
- Click the Instance Number combo box in the New Information column.
- Enter a new computer name or click the down arrow icon for suggestions from the CAF or Device.
Note: Do not assign an Instance Number of 1 to a controller because it is reserved for the tool.
- Specify the changes required for Transfer Operations. See Step 5 in Transferring to a Device for further information.
- Click Finish. When the Transfer to Device completes, your Instance Number is updated.