Transfer Wizard - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Transfer Wizard allows you to transfer a CAF to a device (download) and transfer a CAF to a computer (upload). The Transfer Wizard determines the network connection method by the Connections: Supervisor Passthru, Bluetooth®, MAP 4.2+/BACnet Router, ZigBee, Bluetooth®, or Direct Ethernet network connection methods.