Reliability (WarmupCooldown Sequencing) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Table 1. WarmupCooldown Sequencing Reliability

Input

Behavior When Input Is Not Reliable

Zone Temperature

State is Warmup Unreliable if Mode is Warmup and WarmupCooldown Status is Warmup Unreliable.State is Cooldown Unreliable if Mode is Cooldown and WarmupCooldown Status is Cooldown Unreliable.