Module Use in Applications (WarmupCooldown Sequencing) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual module in this group using the name in the following table.

Table 1. WarmupCooldown Sequencing Uses in Application System Selection Trees

Module Instance Name

Applications

WarmupCooldown Sequencing

VAV Single Duct Applications

VAV Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.