Balancer Override - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Balancer Override modules provides a known interface for external balancing tools to gather data from the VAV application logic and to interact with the application to calibrate the flow calculations. They provide a single point of interface for values that are used in several places in the applications. They also allow the user to configure a subset of that data.

The outputs of this block can be configured by a balancer UI from the tool or a balancing version of the Network Sensor. See the Network Sensor documentation.

You cannot view or modify the modules in this group’s logic.

Important: Do not right-click the State Generation header in the Control View and add a second Balancer Override module because this action breaks the balancing functionality of the application. In addition, do not delete an existing Balancer Override module because this deletion ruins the application.