Module Use in Applications (Balancer Override) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Balancer Override Uses in Application System Selection Trees

Module Instance Name

Applications

Balancer Override DD

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

Balancer Override DDX

VAV Dual Duct Applications (with exhaust box)

VAV Subordinate Dual Duct Applications

Balancer Override SD

VAV Single Duct Applications

VAV Subordinate Single Duct Applications

Balancer Override SDX

VAV Single Duct Applications (with exhaust box)

VAV Subordinate Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.