Attributes (Autocalibration Sequence) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Autocalibration Sequence modules.

Table 1. Autocalibration Sequence Attributes

Name

Description

Default Value

Autocalibrate Now

Specifies that when this value is true, this attribute signals the Flow Calculation modules to calculate a new zero offset.

 

Autocalibration Request

This input is typically connected from the AUTOCAL-C network input (via the Balancer Override modules) to allow a user to manually trigger autocalibration.

False

AUTOCAL-STATE (Autocalibration Status)

Current operational state of the module.

See Primary States (Autocalibration Sequence).

Damper Percent Cmd

Current position of the primary damper. This input is used to verify whether the damper is responding to this module.

0.0

Days between Autocals

Specifies the period between autocalibrations. If set to zero, then periodic autocalibration is not performed. It is set to zero for VAV applications with an exhaust box to prevent disturbing the flow differential controls.

14 days (no Exhaust Box)

0 days (with Exhaust Box)

Eff Stroke Time 1

Specifies the effective stroke time of one of the dampers controlled by the VAV application.

120 Seconds

Eff Stroke Time 2

Specifies the effective stroke time of one of the dampers controlled by the VAV application.

0 Seconds

Eff Stroke Time 3

Specifies the effective stroke time of one of the dampers controlled by the VAV application.

0 Seconds

Output Overridden

Indicates when the controlled outputs are overridden. This stops autocalibration until all damper outputs are not overridden.

False