Module Use in Applications (Last Value) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual State Generation Last Value modules in this group using the names in Table 1.

Table 1. Last Value (Boolean, Enum, Float) Uses in Application System Selection Trees

Module Instance Name

Applications

Pump Startup Required LV

Central Cooling with Optimization Applications

SL Interlock LV

Sideloop Applications

CW Pump Count LV

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.