Attributes (Zone Low Limit Determination) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Zone Low Limit Determination modules.

Table 1. Zone Low Limit Determination Attributes

Name

Type 1

Description

Default Value

ZNLL-DIFF (Low Limit Diff)

 

Specifies that once a low limit state is reached, the zone temperature must increase by this value above the setpoint to return to a normal state.

2 °C, 4 °F

ZNLL-SP (Low Limit Setpoint)

 

Contains the value the zone temperature must go below for it to output a low limit state.

16 °C, 61 °F

ZNLL-STATE (State)

G, V

Indicates whether a low limit condition exists within the zone.

Set Name: Normal/Low Limit

Zone Temperature

 

Current temperature of the zone used to determine if a low limit condition exists.

22 °C, 72 °F

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)