Unit Enable Determination - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module generates a unit enable command. This command is generated from a combination of a network and hardware mode and the parameters for controlling the power fail restart.

You can view and modify the modules in this group’s logic.