The following table describes the attributes used by the System Mode Determination modules:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Eff Mode |
G, V |
Indicates the effective System mode after splitting off the Water Flush output. |
Set Name: Effective System Mode |
|
System Mode |
Indicates the current System Mode. |
Auto Set Name: System Mode |
|
|
Water Flush |
V |
Indicates whether Water Flush is requested. |
Boolean |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)