Primary States (Occupancy Mode Determination [MZ]) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The module behaves in the same manner as the base Occupancy Mode Determination module. The eight Zone X Temp Occ inputs are assumed to be momentary(only active for a few seconds at a time and up to a minute for remote sensors). If an input remains active for long periods of time, the module may not be able to detect other zones requesting temporary occupancy.