Primary States (Fan Alarm Status) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

When the Fan Alarm from the command hierarchy is True the module output is latched in an Alarm state until reset by the reset input.

Table 1. Fan Alarm Status Command Hierarchy

Fan Mode

Flow Status

Fan Alarm

Off

*

False

On

NOT Fault

False

Fault

True