Application Mode Determination - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

AHU applications have an Application Mode input that allows you to force the unit into a mode of operation. The possible modes are Cool Only, Heat Only, Fan Only, Water Flush, Purge, Vent, and Auto. This module separates the Water Flush mode to a separate output to allow it to be separately connected to State Selection.

You can view and modify the modules in this group’s logic.