Attributes (Pass Through) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Pass Through (Boolean, Enum) modules.

Table 1. Pass Through (Boolean, Enum) Attributes

Name

Type 1

Description

Default Value

Input

 

The input to the pass through module.

1st Enum or False

Present Value

G, V

The output of the pass through module

 
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)