Primary States (Occupied Zone Sequencing [VAV]) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
  • Satisfied: The sequencer is in this state when Heating or Cooling are not needed.

  • Supp Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint and Box Priority = Supplemental.

  • Supp Htg + Box Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint, Box Priority = Supplemental, and Supp Heating Control Status = High.

  • Box Heating: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint and Box Priority = Box.

  • Box Htg + Supp Htg: The sequencer is in this state when the Zone Temperature is less than the Heating Setpoint, Box Priority = Box, and Box Heating Control Status = High.

  • Prmy Clg: The sequencer is in this state when the Zone Temperature is greater than the Cooling Setpoint.

  • Temperature Unreliable: The sequencer is in this state when the Zone Temperature is not reliable.