Module Use in Application (Occupied Zone Sequencing [VAV] HFR) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Occupied Zone Sequencing (VAV) HFR Uses in Application System Selection Trees

Module Instance Name

Applications

Occupied Zone Sequencing (VAV) HFR

VAV Dual Duct Applications

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.