Occupied Sequencing (AHU MADD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Occupied Sequencing (AHU MADD) module generates the appropriate temperature control state for the cold deck on a mixed air dual deck Air Handler Unit (AHU) application. This module accepts the temperature and setpoint inputs as well as the heating, cooling, and damper control statuses.