Reliability (Start Stop Sequencing [AHU Mixed Air]) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Table 1. Start Stop Sequencing (AHU Mixed Air) Reliability

Input

Behavior When Input Is Not Reliable

Duct Static Pressure 1

If both Duct Static Pressure 1 and Duct Static Pressure 2 inputs are unreliable, a shutdown Sequence is initiated.

Duct Static Pressure 2

If both Duct Static Pressure 1 and Duct Static Pressure 2 inputs are unreliable, a shutdown Sequence is initiated.