Humidification Sequencing - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module is designed for sequencing the humidification process. While humidifying, the humidification device modulates based on the humidity and the humidity setpoint. This state machine has a limited humidification state for the case where too much moisture is added to the discharge air. This module monitors the status of the zone or return air humidity, discharge air humidity, and setpoints to determine the current humidification control state.

For information on how the FSM determines the state, see FSM (Humidification Sequencing).