The following table describes the attributes used by the Analog Override Check module.
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Number of Input Attributes |
Indicates the number of inputs evaluated by this module. The module calculates this value. |
1 |
|
|
Output n Priority |
Indicates the current priority of the monitored analog output. |
0 Display Precision: 1s |
|
|
Output Overridden |
G |
Indicates whether the output is overridden.This output value is set to True when Setup equals AND, and all of the Output n Priority inputs show that the output objects being monitored are in an Overridden State (that is, the value is greater than zero and less than 16). This output value is set to True when Setup equals OR, and any of the Output n Priority inputs show that the output objects being monitored are in an Overridden State. |
False |
|
Setup |
Indicates whether the value of Output Overridden is set to True when all of the Output n Priority inputs are not 0 or 16 (AND), or this value is set to True when any of the Output n Priority inputs are not 0 or 16 (OR). |
OR Set Name: AND/OR |