System Enable - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The System Enable module enables or locks out a heating or cooling device. This module accepts as inputs outdoor air temperature, outdoor air enable setpoint, outdoor air enable differential, heating/cooling selection, and a network isAvailable. The module has a state output that indicates if the module is enabled.

You can view and modify the modules in this group’s logic.