The following table describes the attributes used by this module.
| Attribute | Type 1 | Description | Default Value |
|---|---|---|---|
| Low Limit Enable |
Indicates the desired setpoint of the PID Pct Cmd. When PID Pct Cmd falls below this setpoint, and if the system is enabled, the output switches to True. |
0.0% | |
| PID Pct Cmd | Represents the variable to which the Low Limit Enable setpoint is compared. | 0.0% | |
| State | Indicates the current operating mode of module. | False | |
| System Enable | Enables the process to run using a True/False command. | False |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)