The following table describes the attributes used by the Plant Sequencing-Building Load modules:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
% Deadband |
Indicates the percentage of the Stage Capacity that separates the Stage Up and the Stage Down. |
5% |
|
|
Control Status |
This returns a status of the System Enable. |
Off |
|
|
Down Delay |
Indicates the minimum time after a Stage Down that another operation (Stage Up or Stage Down) can be performed. |
10 Minutes |
|
|
Load |
Indicates the amount of the load a single stage can satisfy. |
0 btuh or %FLA or Amps |
|
|
Minimum Running Devices |
Indicates the minimum quantity of stages to run as a first stage. |
0 |
|
|
Number of Devices Running |
Indicates the number of devices that are currently being called by the BO sequencer to run. |
0 |
|
|
Output (Float) |
V |
Indicates the number of devices that are being called to run. |
0 |
|
Stabilize Delay |
Prevents debounce in staging up or down. |
180 Seconds |
|
|
Stage Capacity |
Determines whether Stage Up or Stage Down is required and is the variable that is compared to the Stage Capacity and the number of devices running. |
0 btuh or %FLA or Amps |
|
|
Start-Up Delay |
Prevents staging until system reaches equilibrium. |
60 Minutes |
|
|
State |
G |
Indicates the current state. |
Off Set Name: Plant Sequencing Mode |
|
System Enable |
Enables the staging process to run using an Off/On command. |
Off |
|
|
System Interlock Status |
Indicates the status of the interlock. The Global System Interlock Status must be On before any staging can occur. |
On |
|
|
Up Delay |
Indicates the minimum time after a Stage Up that another operation (Stage Up or Stage Down) can be performed. |
15 Minutes |