Module Use in Applications (PID Sequencer) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. PID Sequencer Uses in Application System Selection Trees

Module Instance Name

Applications

CW Sequencing

Central Cooling Applications

CW Sequencing v100

Central Cooling Applications

To see a module's connections and how modules interact with it, view the Connections table.