The following table describes the attributes used by the Device Enable Determination modules:
|
Name |
Type 1 |
Description |
Default Value |
|---|---|---|---|
|
Device Enable n |
Establishes the enable status of the device. A Boolean value of False takes the associated device out of service. If a device is on when this is set to False, Enable n Out is set to False immediately. (Where n is 1-8.) |
True |
|
|
Enable n Out |
G |
Contains the enable value (Boolean) for the corresponding Device. (Where n is 1-8.) |
True |
|
Iso Vlv A Enable n |
Establishes the enable status of an isolation valve. A Boolean value of False takes the associated device out of service. If a device is on when this input is set to False, Enable n Out is set to False immediately. (Where n is 1-8.) |
True |
|
|
Iso Vlv B Enable n |
Establishes the enable status of a second isolation valve. A Boolean value of False takes the associated device out of service. If a device is on when this is set to False, Enable n Out is set to False immediately. (Where n is 1-8.) |
True |
|
|
Pump A Enable n |
Establishes the enable status of a pump. A Boolean value of False takes the associated device out of service. If a device is on when this is set to False, Enable n Out is set to False immediately. (Where n is 1-8.) |
True |
|
|
Pump B Enable n |
Establishes the enable status of a second pump. A Boolean value of False takes the associated device out of service. If a device is on when this is set to False, Enable n Out is set to False immediately. (Where n is 1-8.) |
True |