Device Enable Determination - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Device Enable Determination module enables the device after the required corresponding equipment is enabled and disables the device if any corresponding equipment becomes disabled. For example, when the device is a chiller the corresponding equipment includes condenser isolation valves, condenser pumps, chilled water isolation valves, chilled water pumps, and the chiller itself. This module can also be used to enable one or more towers based on the tower’s corresponding isolation valves.

You cannot view and modify modules in this group’s logic.