Device Availability Calculation (Count True Inputs) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Device Availability Calculation module calculates the number of available devices that are able to run. This module accepts eight device enable inputs as well as a limit input value that acts as a high limit. Based on the input commands and the attribute settings, the module outputs a number (floating value) of devices that are currently available.

You can view and modify the modules in this group’s logic.