Attributes (Device Availability Calculation, Count True Inputs) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following attributes are used by the Device Availability Calculation modules:

Table 1. Device Availability Calculation Attributes

Name

Type 1

Description

Default Value

Device X Enable

 

Indicates if the device is available to run. Device X Enable is a Boolean input.

False

Limit Variable

 

Acts as a high limit in the number of devices that are able to run. Limit Variable is a floating value.

8

Output (Float)

V

Indicates the current number of devices that are able to run.

0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)