Preheat Pump Low OA Alarm - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module provides logic to compare OA-T to a low OALT-SP. When the OA-T is less than the low OALT-SP, the module output matches the value of the Alarm input. When the OA-T is greater than the OALT-SP plus the differential, the output module is in a Normal.

You can view and modify the modules in this group’s logic.