Attributes (Latching Alarm Manager) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Latching Alarm Manager modules:

Table 1. Latching Alarm Manager Attributes

Name

Type 1

Description

Default Value

Cascaded OR Input

 

Provides the functionality to connect multiple modules using the OR operator on more than four inputs.

Normal

Set Name: Normal/Alarm

Input X

 

Indicates the inputs to this module (X is 1-4).

Normal

Set Name: Normal/Alarm

Maintenance Switch

 

Provides the result of the latch and OR operation, but is translated into the disabling/enabling of the maintenance switch.

Enable

Set Name: Disable/Enable

Output

G, V

Provides the result of the latch and OR operation.

Normal

Set Name: Normal/Alarm

Rest X

 

Provides the inputs (X is 1-4) to return the Output to Normal when the Setup X attribute is set to Manual.

Off

Set Name: Off/Reset

Setup X

 

Indicates the latch action used by the specific input (X is 1-4).

When the Setup X attribute is set to Automatic, the Output is Alarm if the associated input is Alarm, and equals Normal when all input values are Normal.

When the Setup X attribute is set to Manual, the Output is Alarm if the associated input is Alarm, and equals Normal when all input values are Normal and the Reset n input is set to Reset.

Automatic

Set Name: Reset Type

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)