Attributes (Dual Fan Alarms) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The following table describes the attributes used by the Dual Fan Alarms modules:

Table 1. Attributes (Dual Fan Alarms)

Name

Typeonr1558008170219.html#onr1558008170219__fn_b_bacnet_exposed

Description

Default Value

Fan 1 Alarm

 

This input represents the alarm condition of the first device.

Default Value: Normal

Set Name: Normal/Alarm

Fan 2 Alarm

 

This input represents the alarm condition of the second device.

Default Value: Normal

Set Name: Normal/Alarm

Output - AND

G

This is the result of the AND operation.

Default Value: Normal

Set Name: Normal/

Output - OR

 

This is the result of the OR operation.

Default Value: Normal

Set Name: Normal/Alarm

1
1

B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)