Viewing and Modifying Parameters - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

You can view and modify parameters or attributes in the Configuration mode, Simulation mode, and Commissioning mode. See Viewing and Modifying Parameters in the Configuring a System section for more information.

Note: System simulation is paused when you transition into Edit mode or open a Command dialog box. Simulation immediately resumes when you exit the window.