Viewing Logic - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

To view logic in the Classic view, click the Logic tab from the user interface. If you are viewing a perspective, add or view the Logic View widget.

Note: If the Logic View widget is already in the perspective, you can also right-click a module containing logic that can be viewed and modified. The right-click menu appears. Select View Logic. The Logic View appears and displays the logic diagram for that module.

You can pan and zoom in the logic view in the Configuration mode, Simulation mode, and Commissioning mode. See Panning and Zooming in the Configuring a System section for more information.

You can print in these modes as well. See Printing the Logic Diagram in the Configuring a System section for more information.