Viewing Connections - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

You can view connections in the Configuration mode, Simulation mode, and Commissioning mode. In Simulation mode, the values are shown in real time rather than defaults. See Viewing and Modifying Connections in the Configuring a System section for more information.