See the Working with Break Conditions section.
| Field | Description |
|---|---|
| Variable | Indicates the break condition object or attribute. |
| Criteria | The standard by which the Value is measured. |
| Value | Indicates the break condition threshold value. |
| Enabled |
Indicates if the break condition is enabled. Note: When a break condition appears during a simulation, the user has the option to click Disable in the dialog box that appears. If the user clicks Disable, then the Enable check box is cleared.
|
|
Add Break Condition |
Saves and closes the Break Condition Details window. |
|
Update Break Condition |
Saves the updated break condition and closes the Break Condition Details window. |
|
Cancel |
Closes the window without applying the changes. |
|
|
Opens the Help system. |
Note: The Active icon (
) is only visible in the Break Condition Detail dialog box when the break condition has been reached through system simulation.